Changer de langue :
With the support of igus, Multipond, a world-renowned specialist for fully automatic multihead weighers, can standardise the bearing materials used. We have also developed a customised linear bearing housing for Multipond, which meets the high requirements of the food industry in terms of design. When every gram counts, numerous food manufacturers rely on the highly automated multihead weighing systems from Atoma GmbH in Waldkraiburg, Bavaria, which markets its systems under the Multipond brand name.
En personne :
Du lundi au vendredi de 8h à 20h. Le samedi de 8h à 12h à Cologne en Allemagne
En ligne :
24h/24