Changer de langue :
Wood dust, high pressure and high temperatures: The environmental conditions for the plain bearings of machines that assemble wood veneers are anything but ideal. Plastic plain bearings from igus® prove themselves under these extreme conditions. Heinrich Kuper GmbH, the only manufacturer worldwide to cover the entire spectrum of veneer assembly technologies, uses split igus® plain bearings made of the material iglidur® G in a new generation of machines at a particularly critical point - the pressure beam bearing.
When it comes to woodworking, German mechanical engineering has a strong position internationally. This may be due in large part to the fact that the material and manufacturing processes place very high demands on the machines and the engineering expertise of the designers. Take veneer production, for example: individual veneer strips are assembled into so-called carpets using high pressing forces and high temperatures.
In addition, the high temperatures that occur lead to thermal expansion, which must also be compensated for by the bearings. Further requirements relate to the ease of servicing and the availability of the bearing and therefore the entire machine: as access to the gluing elements is required for cleaning purposes, the bearing should allow this access - in other words, the beam must be able to move when servicing is required. In addition, the bearings should be largely maintenance-free and wear-free. Last but not least, the costs of the bearings also play a role.
For the ACR - Superquick, Kuper had still provided a translatory pressure beam bearing with ball bushing guides. Michael von Mutius, deputy design manager and project engineer at Heinrich Kuper GmbH responsible for the design of the ACR - Speedstar: "However, this bearing was not maintenance-free and was also relatively expensive. Accessibility to the adhesive elements was also not ideal."
At surface pressures of up to 100 MPa, only negligible plastic deformation is measured with iglidur® G bearings. This high compressive strength was also one of the requirements that Kuper placed on the pressure beam bearing. The bearing is also suitable for accommodating high pressures because the coefficient of friction decreases with increasing load. load but not least, not only the technical but also the economic data are right: iglidur® bearings are significantly more cost-effective compared to commercially available metallic rolled bearings, and of course even more so compared to ball roller bearings. At the same time, the service effort is minimised because the bearings are maintenance-free and have a very long service life: Even at high loads, long-term use with constant friction values is achieved.
Kuper broke new ground with the innovative pressure beam bearing of the ACR-Speedstar and sees this detailed design solution as further confirmation that innovation strengthens competitiveness: The plastic slide bearing has proven itself in practice, and the new generation of machines has already been honoured with the "Challenge Award" at the wood trade fair in Atlanta, USA.