Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Mon interlocuteur
Sélectionner un département
FR(FR)

Maintenance-free plain bearings for 1,028 sun-protection slats in the E.ON technical centre

Corrosion-resistant, lightweight, quiet, and maintenance-free: iglidur J plain bearings in an exterior slat facade

The sun protection facade for the E.ON technical centre consists of 1,028 slats. To keep the workload as low as possible after installation of the huge exterior facade, maintenance-free bearing technology was needed at the vertical slat pivot points. iglidur J plain bearings were chosen because of their incorporated solid lubricants, which allow optimal friction values in the long term – without maintenance.

Profile

  • What was needed: iglidur J plastic bearings
  • Requirements: The bearing points were to be corrosion-resistant and long-lasting. The slats were to be easy to adjust, and the system was to require no maintenance.
  • Industry: facade technology
  • Success for the customer: Thanks to the incorporated solid lubricants in the iglidur plain bearing material, no maintenance is required, and the slats are adjusted almost silently.
Discover all facade technology products
Sun protection cassettes The E.ON technical centre has a great new look. The outer facade boasts 1,028 slats that serve as sun protection for the building.

Problem

To ensure sun protection, a total of 1,026 new slats were installed in the E.ON technical centre in Salzgitter, Germany. The architecturally sophisticated double facade also keeps heat inside the building, contributing to energy conservation. That is why the system is also used in many private and public buildings. The individual slats made of expanded metal are positioned vertically and driven electrically. With an angle of inclination of about 50°, they offer optimum sun protection with a good view of the outside. To implement the complex facade, a solution for slat bearing support at the pivot point was needed. Since the system is exposed to wind and weather, the bearing points had to be corrosion-resistant and durable. They were also to allow easy slat adjustment and require no maintenance. Another consideration was that the more weight to be held or moved, the larger and stronger the construction behind it must be.

Solution

Two plain bearings per slat from the iglidur J plastic bearing product range were installed in the sun-protection facade to adjust the design almost silently over the long term. The bearings can do this because of the incorporated solid lubricants in the plain bearings' iglidur material, which consistently ensures the correct sliding and friction properties for the products. The operator incurs no maintenance or repair costs, since no external grease or lubricants must be added, and system function is always guaranteed.
The very good coefficients of friction allow the slats to adjust smoothly and without jerking in the relatively small amount of installation space they take up. Due to sporadic slat adjustment, no maintenance interval is currently required.

Sun protection cassettes The vertical slats allow an angle of inclination of 50°. iglidur J plain bearings allow entirely lubrication-free, maintenance-free movement.

Go to applied products here


More applications from different sectors can be found here



Les termes "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur" et "xiros" sont des marques protégées de la société igus en République fédérale d'Allemagne et le cas échéant à niveau international.

La société igus signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants de câbles confectionnés pour moteurs indiqués sur ce site Web. Les produits proposés par igus® France sont des produits de la société igus, réservés aux professionnels.