Changer de langue :
motion plastic are high-performance plastics that are used everywhere in industry - and no longer need to be lubricated by users after installation.
This means that not only are expensive greases and oils saved.
Customers also save on maintenance time, labour costs, the risk of incorrect or insufficient lubrication, system downtime and harmful substances that end up in the field or down the drain. We call this: "GO ZERO"

This saves Lemken 22 lubrication points per cultivator.
This saves Huppenkothen 220 maintenance cycles per mini-excavator.
This saves Heineken Brasil up to 28 tonnes of CO2-equivalent per year.

In this white paper, we show which industries and companies are already successfully using lubrication- and maintenance-free bearing technology and the extent to which they benefit from the savings.
Including: Heineken Brasil (beverage technology), KettenWulf (drive and conveyor technology) and Rockinger (agricultural engineering).
Further topics:

... has specialised in the manufacture of agricultural equipment. This includes the Karat 9, an intensive cultivator with tines up to 30 centimetres long. To prevent the tool from being damaged, the tines deflect if too much force is applied - for example by stones in the soil.
Metal bearings were used on all of the tines to ensure the evasive movement. However, the metal bearings had to be lubricated for up to an hour every day. If this was not done, the lack of lubrication would have led to corrosion and wear.
The iglidur® bearings used today work completely without external lubrication, as the material contains self-lubricating solid lubricants. This not only saves the farmer time later on... He also benefits from the high force absorption of the bearing, its lower susceptibility to dirt and an increased downtime of the plain bearings.
Saved lubricant costs
Saved personnel costs
Saved maintenance time
CO saved2-equivalent
Less contaminated freshwater due to pollutants
Less contaminated soil due to pollutant discharge

... with curved, lubrication-free rail guide in the tractor cab.

... with lubrication-free insert on the trailer coupling.

... with robust energy chain for safe guidance of media in dusty and dirty conditions.



... is a supplier of compact excavators, mini excavators and other small equipment and construction vehicles.
In excavators, the bearing points between the stick and excavator bucket are exposed to high forces and harsh environmental influences. Steel bushings are often still used here, which have to be lubricated daily to ensure smooth and low-wear operation.
Four lubrication-free bearings made of high-performance polymer replace the metal bearings at the connection between the stick and bucket. This not only saves 220 maintenance operations per year, but also saves the user high costs for lubricating grease. The risk of insufficient or incorrect lubrication is also reduced.
Saved lubricant costs
Saved personnel costs
Saved maintenance time
CO saved2-equivalent
Less contaminated freshwater due to pollutants
Less contaminated soil due to pollutant discharge

... e.g. with iglidur® G polymer bearings for the lubrication-free arm movement.

... with completely lubrication-free and maintenance-free high-load bearings made of fibre composite material.

... with robust and corrosion-free polymer energy chain for safe guidance of media.



... is the Brazilian branch of a total of 160 branches of the world-famous brewery brand Heineken.
Modern bottling plants can fill up to 70,000 bottles per hour. This process requires a large number of moving parts, such as conveyor technology. Previously, Heinken Brasil had to regularly check and re-grease lubrication points on 600 radial bearings in the conveyor belt.
Polymer bearings are now used in conveyor technology. In future, these will no longer need to be lubricated or serviced during maintenance operations. This saves Heineken Brasil 1,560 hours of maintenance time per year and €2,815.49 in costs just for the lubricating greases saved.
Saved lubricant costs
Saved personnel costs
Saved maintenance time
CO saved2-equivalent
Less contaminated freshwater due to pollutants
Less contaminated soil due to pollutant discharge

... with xiros conveyor roller for lubrication-free conveyor belts.

... with maintenance-free igubal® flange bearings for dry operation.

... with modular and economical Apiro® gearboxes.

*Assumptions for the scaling:
agricultural engineering
Construction machinery
Beverage technology