Mon interlocuteur
Sélectionner un département

igus® E6 system reduces vibrations

The E6 series satisfies through its modular design, which enables the chain to be shortened or lengthened at the required position. The special structure of the chain link and the small division grant an extremely quiet and low-vibration operation of the chain. The E6 series is available as open chain or enclosed tube.

Vibration reducing e-chain® systems lying on top of each other reduce vibrations and enhance cutting accuracy, here the E6.80 series at the company Dörries Scharmann Technologie GmbH.

Further interesting applications from extremely diverse areas can be found here